Q.1: Is there anyone having the same problem as below?
"generate/include/Flexio_Pwm_Ip_Cfg.h:54:10: fatal error: Flexio_Pwm_Ip_BOARD_InitPeripherals_PBcfg.h: No such file or directory"
I thought this message means I have done something wrong. But, this problem is easily solved if I correct header include statement manually (to Flexio_Pwm_Ip_PBcfg.h).
Q.2: What is wrong with template file (of Flexio_Pwm_Ip_Cfg.h) or my configuration?
(I have check my c-code. It will run just fine if the wrong include statement is fixed manually.)
解決済! 解決策の投稿を見る。
Hi
Please try to test whether the latest S32K3 RTD 4.0.0 has fixed this issue.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
Please try to test whether the latest S32K3 RTD 4.0.0 has fixed this issue.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Yes. These two packages are actually the same, only the name was changed from MAXQFP to HDQFP.