Clock configure for S32K116 by S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock configure for S32K116 by S32DS

470件の閲覧回数
547416104
Contributor III

Hello Everyone,

I just use S32DS to configure clock for S32K116 (48 PIN), and there is no "SPLL_CLK" item listed in Clock sources, but refer to the datasheet, SPLL_CLK clock source is supported, whether need to configure other items for enable the SPLL_CLK clock source?

Thanks for your attention!

S32K116 48pin.png

0 件の賞賛
1 返信

464件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

There is no PLL in S32K11x. You can find the information in S32K1xx MCU Family - Reference Manual and AN11997: Differences Between S32K11x and S32K142 – Application Note.

Figure 27-1. Clocking diagram S32K11x SPLL.pngTable 1. Core and system differences.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛