Change the IO voltage of s32K3X4EVB-Q257 development board to 3.3V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Change the IO voltage of s32K3X4EVB-Q257 development board to 3.3V

跳至解决方案
1,171 次查看
TZYlss
Contributor I

Hello, I want to change the IO voltage of S32K3X4EVB-Q257 development board to 3.3V, what should I do

0 项奖励
回复
1 解答
1,144 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi TZYlss,

Please refer S32K3 MCUs for General Purpose – Hardware Design Package and S32K3X4EVB-Q257 and Q257ND Evaluation Board – HW User Manual

VDD_HV_A VDD_HV_B IO Supply Voltage.pngVDD_HV_A.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,145 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi TZYlss,

Please refer S32K3 MCUs for General Purpose – Hardware Design Package and S32K3X4EVB-Q257 and Q257ND Evaluation Board – HW User Manual

VDD_HV_A VDD_HV_B IO Supply Voltage.pngVDD_HV_A.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------