Change the IO voltage of s32K3X4EVB-Q257 development board to 3.3V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change the IO voltage of s32K3X4EVB-Q257 development board to 3.3V

ソリューションへジャンプ
1,179件の閲覧回数
TZYlss
Contributor I

Hello, I want to change the IO voltage of S32K3X4EVB-Q257 development board to 3.3V, what should I do

0 件の賞賛
返信
1 解決策
1,152件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi TZYlss,

Please refer S32K3 MCUs for General Purpose – Hardware Design Package and S32K3X4EVB-Q257 and Q257ND Evaluation Board – HW User Manual

VDD_HV_A VDD_HV_B IO Supply Voltage.pngVDD_HV_A.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,153件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi TZYlss,

Please refer S32K3 MCUs for General Purpose – Hardware Design Package and S32K3X4EVB-Q257 and Q257ND Evaluation Board – HW User Manual

VDD_HV_A VDD_HV_B IO Supply Voltage.pngVDD_HV_A.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------