Hello everyone
When I use PE to debug the FTM IC peripherals, if I run directly without setting breakpoints, the function is normal. It doesn't work when a breakpoint is set and the program is stopped and then run. Run directly after reset, and the function is restored.
FTM Global config:Debug mode is Mode3;
Can you try seting the debug mode to 0x00?
FTM_BDM_MODE_00 = 0x00U, /*!< FTM counter stopped, CH(n)F bit can be set, FTM channels
* in functional mode, writes to MOD,CNTIN and C(n)V registers bypass
* the register buffers */
FTM_BDM_MODE_01 = 0x01U, /*!< FTM counter stopped, CH(n)F bit is not set, FTM channels
* outputs are forced to their safe value , writes to MOD,CNTIN and
* C(n)V registers bypass the register buffers */
FTM_BDM_MODE_10 = 0x02U, /*!< FTM counter stopped, CH(n)F bit is not set, FTM channels
* outputs are frozen when chip enters in BDM mode, writes to MOD,
* CNTIN and C(n)V registers bypass the register buffers */
FTM_BDM_MODE_11 = 0x03U /*!< FTM counter in functional mode, CH(n)F bit can be set,
* FTM channels in functional mode, writes to MOD,CNTIN and C(n)V
* registers is in fully functional mode */