Can't use PEmicro debugger with S32K3X4EVB-T172

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't use PEmicro debugger with S32K3X4EVB-T172

Jump to solution
549 Views
Jimmy18x2
Contributor II

I have a problem about the PEmicro in Step 4.3 Upload Software and Debug. 

Getting Started with the S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose 

 

Error in services launch sequence
PEmicro GDB Launch Failure : The GDB Server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch settings in the Debug Configuration are accurate.

2.PNG

 

This Can't use PEmicro debugger with S32K118EVB2-Q048 showed Kinetis_Recovery_Utility.zip how  to make sure that the PEmoicro is work, but the figure of my computer shows that PEmicro is still not work.

1.PNG

This blew figure shows my installed softwares and drivers.

3.PNG

In additional, why is the LED RST_OSDA always high not blink.

EVM.jpg

Tags (2)
0 Kudos
Reply
1 Solution
524 Views
Jimmy18x2
Contributor II

After Plugging in the Power Supply with a transfer with supported 12 V, the User LED is blinking.

Remember that the EVM must support it with a external voltage.

View solution in original post

0 Kudos
Reply
1 Reply
525 Views
Jimmy18x2
Contributor II

After Plugging in the Power Supply with a transfer with supported 12 V, the User LED is blinking.

Remember that the EVM must support it with a external voltage.

0 Kudos
Reply