Can't see the expressions during runing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't see the expressions during runing

2,123 Views
shey_alex
Contributor II

Hello,

I've just downloaded one of the program examples to S32K144. In debug mode i added some variables to watch window, however i was unable to watch their changes while the program is running, only if i stop, i can see the current value of the variable. Is there any settings where i can unlock this feature? or changes of the variables originally can't be seen in debug mode watch window?

Thanks a lot.

0 Kudos
Reply
1 Reply

2,023 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

one colleague of mine has been solving this issue. Please see the link below, it could be useful for you.

https://community.nxp.com/thread/454004 

Regards,

Martin

0 Kudos
Reply