Can't install S32K3xx Development Package and FreeMASTER Serial Communication Driver version 1.3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't install S32K3xx Development Package and FreeMASTER Serial Communication Driver version 1.3.0

Jump to solution
754 Views
Jimmy18x2
Contributor II

I have received the S32K3X4EVB-T172. 

Question 1: When I tried install the S32DS 3.5.9, I could't  install the S32K3xx Development Package by SW32_S32DS_3.5.9_D2312.zip only showed S32 Design Studio Platform Package and S32 Design Studio Platform Tools Package

2. Get Software: 2.2 Install the S32K3xx Development Package 

Open About S32 Design Studio for S32 Platforms dialog (menu → Help → About S32 Design Studio for S32 Platforms) shows the following as:

S32 Design Studio for S32 Platform
Version: 3.5
Build id: 231219 (Update 9)

Question 2: I have already installed the FreeMASTER 1.3.0 RTM (FMASTERSW32.exe) in Step "2.4 Get the Run-Time Debugging Tool", but I can't install "FreeMASTER Serial Communication Driver version 1.3.0" on S32DS Extensions and Updates dialog (menu → Help → S32DS Extensions and Updates). 

The error message shows as following as:

Operation details Software being installed: com.nxp.s32ds.s32k3.sdk.freemaster.feature.feature.group 1.3.0.202312191400 Missing requirement: com.nxp.s32ds.s32k3.sdk.freemaster.feature.feature.group 1.3.0.202312191400 requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.s32k3.dev.feature.feature.group 1.0.0' but it could not be found.

The installation Details:

Package: GDB Client for Arm Embedded Processors 12.1 Build 1702; Version: 1702; Build id: 202309251304
Package: S32 Design Studio Platform package; Version: 3.5.9; Build id: 202312191958
Package: S32K3 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202303311831
Package: S32K3.P01 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202304031555
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.1.7; Build id: 202112141853
Package: S32 Design Studio Platform Tools package; Version: 3.5.9; Build id: 202312191958
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
Package: S32 Design Studio Debugger Core; Version: 3.5.9; Build id: 202312191723

Tags (1)
0 Kudos
Reply
1 Solution
707 Views
Jimmy18x2
Contributor II

I have install the FreeMASTER 1.3.0 RTM (FMASTERSW32.exe) after that i had installed the S32K3xx Development Package from SW32K3xx_S32DS_3.5.0_D2303.zip (Upload from previous version S32DS 3.5.3).

View solution in original post

0 Kudos
Reply
1 Reply
708 Views
Jimmy18x2
Contributor II

I have install the FreeMASTER 1.3.0 RTM (FMASTERSW32.exe) after that i had installed the S32K3xx Development Package from SW32K3xx_S32DS_3.5.0_D2303.zip (Upload from previous version S32DS 3.5.3).

0 Kudos
Reply