Can not see anything in register view when using jlink.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not see anything in register view when using jlink.

ソリューションへジャンプ
1,614件の閲覧回数
郑文豪
Contributor I

When I using j-link debug s32k144,it is empty in peripheral registers values and peripheral register windows.It is ok in using usb link.

0 件の賞賛
返信
1 解決策
1,601件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 郑文豪,

If you are using S32DS IDE, please try to use the EmbSys Registers window.

SEGGER J-Link Debugging.pngEmbSys Registers.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,602件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 郑文豪,

If you are using S32DS IDE, please try to use the EmbSys Registers window.

SEGGER J-Link Debugging.pngEmbSys Registers.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,595件の閲覧回数
郑文豪
Contributor I

There is no value.

573482CD-6ACE-4505-90D0-D2C7D6730D93.png

0 件の賞賛
返信
1,591件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Double click on register to read values, after that the register names will shown green.

0 件の賞賛
返信
1,582件の閲覧回数
郑文豪
Contributor I

Thank you !

0 件の賞賛
返信