Can not open the example from SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not open the example from SDK

2,399 Views
Hermit
Contributor I

Hi Team,

When I want to open a example project from SDK, I can open it successfully by S32DS,however, I can not open the ".mex" file.It shows that the pins tool was forbidden.

Then, I open the pins tool,but there is no pins that is configured in advance. Also, there is something wrong with the peripheral tools.It just shows that It can not find the drivers in toolchains or IDE and the project can not be compiled.

0 Kudos
Reply
2 Replies

2,392 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Hermit 

please click the Update Code button then you can build the demo successfully!

Senlent_1-1673235983207.png

This demo set the FlexCAN to Loop-Back mode, so it doesn't enable pins tool.

0 Kudos
Reply

2,389 Views
Hermit
Contributor I

Hi Senlent,

Thanks.

0 Kudos
Reply