Can not debug S32K144EVB with PEMicro multilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not debug S32K144EVB with PEMicro multilink

1,563 Views
lwcall2007
Contributor I

I use S32K144EVB to study S32K144 , i can debug S32K144 with OpenSDA , but fail to debug it with my PEMicro multilink device

0 Kudos
3 Replies

1,528 Views
JustVb
Contributor III

I met the same problem,maybe there is something wrong with your debugger hardware.

I used another debugger, the problem was solved.

0 Kudos

1,551 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi lwcall2007,

Please notice the 1st pin of SWD CONNECTOR(J14), red line should be connect at 1st pin.

SWD CONNECTOR J14.jpg

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,543 Views
lwcall2007
Contributor I

I have tried to exchange the SWD pin connection , but it still does not work

0 Kudos