Can not creat a project with S32K342

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not creat a project with S32K342

3,491件の閲覧回数
Hermit
Contributor I

Hi Team,

I want to creat a new project with S32K342, but I failed. There is no S32K342 chip for me to choose(I attached a screenshot below). 

The version of S32DS is V3.4 and the version of RTD SDK is "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204". By the way, I can not open the example where S32K342 is used. There is no example for S32K342! I attached it below.

Need I configure the S32DS or add some special packages to make it applicable to S32K342?

0 件の賞賛
返信
4 返答(返信)

3,478件の閲覧回数
Hermit
Contributor I

Thank you

0 件の賞賛
返信

3,483件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure right development package is installed into S32DS.

PetrS_0-1673948805896.png

I can see S32K342 option when creating new project

PetrS_1-1673948843804.png

There are examples for S32K342 within RTD package

PetrS_2-1673949469782.png

BR, Petr

 

0 件の賞賛
返信

2,539件の閲覧回数
fan1234
Contributor II

Hi, PetrS

 I can see S32K342 option when creating new project but there are examples for S32K342 within RTD package. can you help me with that?

The version of S32DS is V3.5  and the extension are:

fan1234_0-1733983230675.png

and i checked, thedevelopment package is installed

fan1234_2-1733983461366.png

 

thank you.

タグ(1)
0 件の賞賛
返信

2,534件の閲覧回数
fan1234
Contributor II
sorry, made a mistake,it should be " there are no examples for S32K342 within RTD package".
0 件の賞賛
返信