Can S32K3XX support open alliance SPI protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can S32K3XX support open alliance SPI protocol

Jump to solution
1,640 Views
Deryck_Tsui
Contributor I

Hello NXP,

        I need use the MAC-PHY transceiver in Ethernet communication which support OA-SPI(Open Alliance SPI) interface. No relerant information was found. Can give me some information about it, thank you for your help.

The document link: OPEN Alliance 10BASE-T1x MAC-PHY Serial Interface (opensig.org)

Tags (1)
0 Kudos
Reply
1 Solution
1,591 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, it generally looks like standard SPI communication, so LPSPI module would be able to handle that. But given protocol has to be done by own.

BR, Petr

View solution in original post

0 Kudos
Reply
2 Replies
1,592 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, it generally looks like standard SPI communication, so LPSPI module would be able to handle that. But given protocol has to be done by own.

BR, Petr

0 Kudos
Reply
1,567 Views
Deryck_Tsui
Contributor I
Ok, I got it. Thanks for your reply
0 Kudos
Reply