Can I erase a Phrase (8-byte/64-bit) before program (write) phrase operation for Data Flash in S32K144 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I erase a Phrase (8-byte/64-bit) before program (write) phrase operation for Data Flash in S32K144 ?

1,853件の閲覧回数
nitinverma
Contributor III

Hello lukaszadrapa,jirikral‌ and danielmartynek,

I would like to inform that I am using entire FlexNVM as Data Flash in S32K144 freedom board. I have a application to write only 8-byte in DFlash whenever it's required. For that, I need to erase only 8-byte before write operation. I can write required 8-byte with 'Program Phrase' command available in Flash Driver however I did not find any relative 'Erase Phrase' command for 8-byte erase operation. 'Erase Flash Sector' command does not allow to erase lesser than 2 KB and 'Erase Flash Block' command is erasing entire DFlash of 64 KB.

Please let me know if it's possible to erase 8-byte only at a time and also if I am not doing it correctly.

Thank You ! :smileyhappy:

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,643件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Nitin,

Unfortunately, this is not possible.

The smallest portion of D-Flash that can be erased is the 2K sector.

Regards,

Daniel

0 件の賞賛
返信

1,643件の閲覧回数
nitinverma
Contributor III

:smileysad:. Anyways thanks a lot Daniel for your prompt response.

0 件の賞賛
返信