Hi,
Can I disable S32K3's JTAG permanently (no secure debugging) by LifeCycle configuration bit without writing a ADKP?
In the S32K3 RM Table 704 “Debug access based on LifeCycle and bit configurations”.
Does it mean I can change the LifeCycle setting to IN_FIELD in the application code and tell HSE to burn the fuse to disable the JTAG permanently without ADKP (i.e. no secure debugging)?
Regards,
Snaku
已解决! 转到解答。
Hi @snaku_lee,
Unfortunetely, it is not possible to disable it permanently.
it will be always possible to disable the secure debug by the password.
BR, Daniel
Hi @snaku_lee,
It is possible to restrict the debug access via the password protection when HSE is not used.
You need to program the CUST_DB_PSWD_A field in UTEST with the desired password and then advance the lifecycle.
In order to advance the lifecycle:
1) Set the address of LC configuration word in the IVT/bootheader. LC word can be at any flash address selected.
2) Write in such address the value for LC word corresponding to target lifecycle:
BR, Daniel
Hi Daniel,
Thanks for your reply.
Our customer request us to disable JTAG permanently without password, nor ADKP.
They don't want a backdoor on JTAG.
Is that possible to disable S32K3 JTAG by the LifeCycle fuse?
Regards,
Snaku
Hi @snaku_lee,
Unfortunetely, it is not possible to disable it permanently.
it will be always possible to disable the secure debug by the password.
BR, Daniel