CAN0 FD‘s BRS&ESI&DLC waveform is strange

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN0 FD‘s BRS&ESI&DLC waveform is strange

Jump to solution
1,957 Views
chengsz1206
Contributor II

According to  CAN FD spec,the BRS+ESI+DLC is 6bit。

But their waveform is not 6bit。I find the waveform  is strange。

The wave form is as follow。Who can help me?

FD.PNG

For details,please refer to CAN FD _issue.xlsx。

1 Solution
1,886 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the waveform is correct.

The bit meaning of the CANH signal is below

CAN fd frame1.png

when zooming into bitrate switching...

CAN fd frame 2.png

At the sample point of BRS bit the bitrate is switched, so BRS bit is little bit shorter then previous bits.

Within DLC bits a stuff bit of opposite polarity is inserted after five bits of same polarity are detected.  

BR, Petr

View solution in original post

1 Reply
1,887 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the waveform is correct.

The bit meaning of the CANH signal is below

CAN fd frame1.png

when zooming into bitrate switching...

CAN fd frame 2.png

At the sample point of BRS bit the bitrate is switched, so BRS bit is little bit shorter then previous bits.

Within DLC bits a stuff bit of opposite polarity is inserted after five bits of same polarity are detected.  

BR, Petr