CAN_PAL thoughput with S32K14x at 1Mbps

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN_PAL thoughput with S32K14x at 1Mbps

1,249 Views
yfliu
Contributor IV

Hi,

I am wondering where we can find CAN_PAL program throughput test data (in bps) with 1Mbps CAN bus? 

Test program shall use CAN_PAL api on S32K14x device.

- Loopback throughput: one S32K14x in loopback mode.

- Two S32K14x devices (1 sender and 1 receiver) on a CAN bus.

Regards,

Yanfeng

 

 

 

 

 

0 Kudos
6 Replies

1,176 Views
Brunner35
Contributor I

This application note provides software examples and
describes necessary startup steps needed to help users get
started with S32K1xx series MCUs.

0 Kudos

1,223 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Yanfeng,

I am sorry to tell you that we did not offer throughput test data.
Maybe you can have a test by using CAN analyzer.

Best Regards,
Robin

0 Kudos

1,209 Views
yfliu
Contributor IV

Robin,

 

Thanks for the information.

Here we did a simple test on S32K146EVB, using loop back mode with FreeRTOS.

The initializer sets up CAN_PAL device in loopback mode, and sets speed as 1Mbps, installs our ISR callback. Then it starts two test tasks, which contain the following loops:

- Sender loop:  1) call CAN_Send() API, 2) wait for txSemaphore;

- Receiver loop: 1) call CAN_Receive() API, 2) wait for rxSemaphore;

In our CAN_PAL callback, we notify the txSemaphore or the rxSemaphore accordingly.

However, the throughput we got is about 1000mps for both sender and receiver tasks. Given we are using 8 byte standard CAN message, this is about 110kbps, far from the 1Mbps value. 

Can you please share what was missed here?

 

Regards,

Yanfeng

 

 

 

 

 

0 Kudos

1,201 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

What Bitrate did you set for the Arbitration Phase and Data Phase?(The CAN_PAL demo set 500 kbit/s by default)

Bitrate.jpg

Data frame CAN.jpg

0 Kudos

1,184 Views
yfliu
Contributor IV

Robin,

 

The bitrate we are using is 1000kbps as mentioned in the subject .

 

Regards,

Yanfeng

 

0 Kudos

1,165 Views
yfliu
Contributor IV

Thanks a lot, @Robin_Shen  and @Brunner35 for your comments.

We've achieved about 600Kbps in loopback mode now after tweaking task synchronisations. If there is a way to achieve higher throughput, please teach. 

0 Kudos