Building S32K344 project in S32DS3.4 take more than 5min ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building S32K344 project in S32DS3.4 take more than 5min ?

840 Views
phidiawang
Contributor III

Hi,

I built  a S32K344 project in S32DS3.4,and it took me for more than 5min.Can I speed up it ?thanks.

微信图片_20220104134435.png

Tags (1)
0 Kudos
Reply
3 Replies

817 Views
phidiawang
Contributor III

Senlent:

thanks. I modifed that setting as you said,but it is still very slow.

0 Kudos
Reply

806 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@phidiawang

    I have also encountered a situation that can reduce the build-time,which is disconnecting the network,because the S32 DS background update tasks will increase the burden of the CPU, maybe you can try this method is effective to you or not.

BR!

     Jim,

0 Kudos
Reply

828 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@phidiawang

There some tips may help you speed up your build time.

 

Fist, you can close the unused project ,as I can see that you opened many unused projects,and then try to clean the project you using,then build it again.

 

Second,try to expand the max heap size of S32 DS.

please try to click below link for details.

https://community.nxp.com/t5/S32K/How-to-expand-the-max-heap-size-of-s32ds/td-p/1379575 

BR!

     Jim,

 

0 Kudos
Reply