Build error "first defined here" of iseled s32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build error "first defined here" of iseled s32k144

1,271 Views
nanjun
Contributor III

Hello,

Build process failed in project  iseled_freemaster_s32k144.

Error.PNG

Few minutes ago it still worked as expected. I am not sure where I modified in SDK. Is this any error regarding project configuration?

Kind regards,
Neo

0 Kudos
8 Replies

1,004 Views
toxuandung
Contributor I

Hi nanjun,

I try to install S32 SDK ISELED driver but I can only download the version as picture bellow.

Can I ask you one question that which version of S32 SDK ISELED driver you use.

Thanks you !

 

toxuandung_0-1671003451934.png

 

0 Kudos

996 Views
nanjun
Contributor III

Hello,

I did not use Autosar instead the RTM SDK v3.0.0 was installed.

Kind regards,

Nanjun

0 Kudos

991 Views
toxuandung
Contributor I

Hi nanjun,

Thanks you so much for the reply.

RTM SDK IESLED v3.0.0 driver is the version I want to install but I not able to find that in NXP website.

Could you please help to send me the installation file aslo the license file if you can download from NXP.

0 Kudos

984 Views
nanjun
Contributor III

Hello,

could you follow the 1.5 section to download it? The driver is too large to upload.

https://www.nxp.com/document/guide/get-started-with-the-s32k-iseled:GS-S32K-ISELED

The guide can be found here:

https://www.nxp.com/docs/en/user-guide/S32KSDKISELEDRTMUG.pdf

0 Kudos

972 Views
toxuandung
Contributor I

Hi nanjun,

Please have look at the pictures bellow. Actually I already try many time to follow the guide from NXP but I still not able to download the driver. Can you please help to send me by wetransfer.

Thanks you so much for the strong support. I am stuck with my project now.

toxuandung_1-1670465321035.png

toxuandung_2-1670465346667.png

toxuandung_4-1670465397645.png

toxuandung_5-1670465432328.png

0 Kudos

1,267 Views
nanjun
Contributor III

Moreover, the error is shown like this:

Building target: iseled_freemaster_s32k144.elf
Executing target #42 iseled_freemaster_s32k144.elf
Invoking: Standard S32DS C Linker
arm-none-eabi-gcc -o "iseled_freemaster_s32k144.elf" "@iseled_freemaster_s32k144.args"
./SDK/platform/drivers/src/lpspi/lpspi_master_driver.o:C:/nxp/S32DS_ARM_v2018.R1/S32DS/S32SDK_S32K1xx_RTM_3.0.0/platform/drivers/src/lpspi/lpspi_master_driver.c:112: multiple definition of `exit_code'
XXX\ise_ctl\iseled_freemaster_s32k144\Debug_FLASH/../Sources/main.c:115: first defined here

 

like Multiple+first define error.

0 Kudos

1,241 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

can't really say, this is not easy question if something was changed by accident. Is it possible to share the project?

Regards,

Lukas

0 Kudos

1,209 Views
nanjun
Contributor III

Hello Lucas,

thanks for your reply. Attached you find the project. Actually, with the solution from here the problem can be solved, but it was not required previously.

Kind regards,

Nanjun Xu

 

 

0 Kudos