Boundary scan on S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boundary scan on S32K144

Jump to solution
860 Views
JosefFuchs
NXP Employee
NXP Employee

Hello,

 

when using Boundary scan on S32K144, is there any signal required on one of the 4 JTAG pins to enable Boundary Scan mode?
e.g. is it required to pull one of the four signals high or low during (or after) RESET to enable the interface?
or is the default state of the pins (using internal pulls) ok for using boundary scan?

Thanks,
Josef

Tags (2)
0 Kudos
1 Solution
850 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Josef,

the debug port comes out of reset in standard JTAG mode which is used for boundary scan, so no special configuration is needed. Default configuration of the pins is ok.

Regards

Lukas

View solution in original post

0 Kudos
1 Reply
851 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Josef,

the debug port comes out of reset in standard JTAG mode which is used for boundary scan, so no special configuration is needed. Default configuration of the pins is ok.

Regards

Lukas

0 Kudos