Boundary scan on S32K144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Boundary scan on S32K144

跳至解决方案
859 次查看
JosefFuchs
NXP Employee
NXP Employee

Hello,

 

when using Boundary scan on S32K144, is there any signal required on one of the 4 JTAG pins to enable Boundary Scan mode?
e.g. is it required to pull one of the four signals high or low during (or after) RESET to enable the interface?
or is the default state of the pins (using internal pulls) ok for using boundary scan?

Thanks,
Josef

标记 (2)
0 项奖励
1 解答
849 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Josef,

the debug port comes out of reset in standard JTAG mode which is used for boundary scan, so no special configuration is needed. Default configuration of the pins is ok.

Regards

Lukas

在原帖中查看解决方案

0 项奖励
1 回复
850 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Josef,

the debug port comes out of reset in standard JTAG mode which is used for boundary scan, so no special configuration is needed. Default configuration of the pins is ok.

Regards

Lukas

0 项奖励