Hi @nxp
We have currently working on Multicore booting S32k322 MCU in following packages in GHS SW32K3_S32M27x_RTD_4.4_4.0.0_P24.
Failure Case:
When attempting dual-core execution in GHS, we are facing issues with both cores running properly. The summary is as follows:
Please help us on this, since the startup file is part of the MCAL package and we are not authorized to modify or touch anything inside the MCAL SIP.
We requested SW32K3_S32M27x_RTD_4.4_4.0.0_P24 - Bare metal dual-core code that can boot and reach the main function in GHS using the MCAL package.
Thank you!
Vivek Arivazhagan
Can you share the project so that we can test it?
If you don't want to share it here, please create a support ticket.
Regards,
Daniel
Hi @jiri_kral ,
Thanks for sharing. Based on our observation, the project currently has a dual setup with two projects, two ELF files, and two startup files. However, our expectation is to have a single project with one startup file and a single ELF file, with all source files managed within GHS.
Kindly help us with this. You may either make the necessary changes to the project we shared for your reference or provide a version that meets these expectations.
Note: we are stuck with how to wait core 1 until core 0 initialized. kindly support on this also
Thanks,
Vivek Arivazhagan
.