BCC_S32K144_Monitoring example requires KSDK 1.1 but the Kinetis SDK path opthon refers to SDK_S32K1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BCC_S32K144_Monitoring example requires KSDK 1.1 but the Kinetis SDK path opthon refers to SDK_S32K1

Jump to solution
994 Views
Zyuan17
Contributor III

Hi,

I am using S32K DS 2018.R1 to run the BCC monitoring example (using MC33771C). And there is a window pop-up shows that this project runs on the Kinetis SDK not my current SDK. I then choose continue. The software told me to change the SDK. What should I choose?

 

Zyuan17_0-1666717730215.pngZyuan17_1-1666717741456.png

 

0 Kudos
1 Solution
984 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Zyuan17,

Did you follow the UM11346 and then install the S32 Design Studio for ARM 2018.R1 - Update 11?

UM11346 Installing IDE.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
7 Replies
889 Views
Zyuan17
Contributor III

The problem is solved. The simplest way is just to install all the SDKs.

0 Kudos
985 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Zyuan17,

Did you follow the UM11346 and then install the S32 Design Studio for ARM 2018.R1 - Update 11?

UM11346 Installing IDE.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
979 Views
Zyuan17
Contributor III

Zyuan17_0-1666770780533.png

yes I did, the 3.0.2 update is already installed

 

0 Kudos
948 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

After uninstalling and reinstalling S32DS, I offline install(Help->Install New Software) the whole S32DS_ARM_v2018.R1_UP11.zip.

As you can see the I select all, and all these turned grey.

Help Install New Software S32DS_ARM_v2018.R1_UP11.png

This is yours:

black.png

The Selected SDK path of mine is C:\NXP\S32DS\....(I install S32DS in C drive.)

path.png

Tags (1)
0 Kudos
966 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I am able to build this project without error. Let me try uninstalling and reinstalling S32DS to see which SDK package is required.

without error.png

 

0 Kudos
357 Views
zq1
Contributor III

 i am using MC3772C tpl with  MC3364 recently, so i need some documents and help about ,could you please tell me where i can find the examples or other documents ,thank you 

0 Kudos
961 Views
Zyuan17
Contributor III

Zyuan17_0-1666785064515.png

 

 

As you can see, the SDKs are already installed.

0 Kudos