Hi,
I am using S32K DS 2018.R1 to run the BCC monitoring example (using MC33771C). And there is a window pop-up shows that this project runs on the Kinetis SDK not my current SDK. I then choose continue. The software told me to change the SDK. What should I choose?
Solved! Go to Solution.
Hi Zyuan17,
Did you follow the UM11346 and then install the S32 Design Studio for ARM 2018.R1 - Update 11?
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
The problem is solved. The simplest way is just to install all the SDKs.
Hi Zyuan17,
Did you follow the UM11346 and then install the S32 Design Studio for ARM 2018.R1 - Update 11?
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
yes I did, the 3.0.2 update is already installed
After uninstalling and reinstalling S32DS, I offline install(Help->Install New Software) the whole S32DS_ARM_v2018.R1_UP11.zip.
As you can see the I select all, and all these turned grey.
This is yours:
The Selected SDK path of mine is C:\NXP\S32DS\....(I install S32DS in C drive.)
I am able to build this project without error. Let me try uninstalling and reinstalling S32DS to see which SDK package is required.
As you can see, the SDKs are already installed.