Ask for help about S32K144 application of FTM0-PDB1-ADC1 sequence error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ask for help about S32K144 application of FTM0-PDB1-ADC1 sequence error

1,022 Views
jxl
Contributor I

Dear sir,

      Can you help me about ADC1 convert time in S32K144? 

I follow the link below,https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/s32k144-PWM-to-ADC-sync/m-p/1032279#M4217 , configured my FTM0/PDB1 to trigger ADC1, attemp to sync adc1 convert data to a PWM signal(100KHz) which generated by FTM0.

   My code as below:

int main(void)

{

ftm_state_t ftmStateStruct;


CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);


PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);

 

TRGMUX_DRV_Init(INST_TRGMUX1, &trgmux1_InitConfig0);

PCC->PCCn[PCC_PDB1_INDEX] |= PCC_PCCn_CGC_MASK; /* Enable bus clock in PDB1 */

PDB_DRV_Init(INST_PDB1, &pdb1_InitConfig0);
PDB_DRV_Enable(INST_PDB1);

// config 8 pretriggers on ch0 based on component setting
PDB_DRV_ConfigAdcPreTrigger(INST_PDB1, 0UL, &pdb1_AdcTrigInitConfig0);


PDB_DRV_SetTimerModulusValue(INST_PDB1, 30);    // 
// set ch0 trigger0 delay to happen immediate upon Trigger_In 0 (PIT0 ch0)
PDB_DRV_SetAdcPreTriggerDelayValue(INST_PDB1, 0UL, 0UL, 30);

//PDB_DRV_SetCmpPulseOutDelayForHigh(INST_PDB1, 0L , 0);
//PDB_DRV_SetCmpPulseOutDelayForLow(INST_PDB1, 0L, 75);
//PDB_DRV_SetCmpPulseOutEnable(INST_PDB1, 1<<0, true);
PDB_DRV_LoadValuesCmd(INST_PDB1);


INT_SYS_InstallHandler(PDB1_IRQn, &PDB1_IRQHandler, (isr_t *)0);
INT_SYS_EnableIRQ(PDB1_IRQn);

ADC_DRV_ConfigConverter(INST_ADC1, &adc1_ConvConfig0);
ADC_DRV_ConfigChan(INST_ADC1,0, &adc1Channel)


FTM_DRV_Init(INST_FLEXTIMER_PWM1, &flexTimer_pwm1_InitConfig, &ftmStateStruct );
FTM_DRV_InitPwm(INST_FLEXTIMER_PWM1, &flexTimer_pwm1_PwmConfig);

INT_SYS_InstallHandler(ADC1_IRQn,&ADC1_IRQHandler,(isr_t *)0);
INT_SYS_EnableIRQ(ADC1_IRQn);


INT_SYS_EnableIRQGlobal();

while(1)

{

}

 

}

void ADC1_IRQHandler()
{

ADC_DRV_GetChanResult(INST_ADDEMOD, 0, &ADC1_res);
convert_success = TRUE;

}

 

void PDB1_IRQHandler(void)
{
//PDB1->SC &= ~0x00000040; //PDBIF w0c
if((PDB1->CH[0].S & 0x00000001)==0x1)
{
PDB1->CH[0].S &= 0xFFFFFFFE;
}
}

PDB1 delay = 1/48MHz * 30 = 0.625us

ADC1 Clock = 48M,  SMPLTS=12, 8-bit Mode, No HW average, ONLY sample one channel. According to S32K-RM, ADC Convert time = (12+1)+1+20+5+5 = 38 ADC cycles + 5 bus clock cycles = 43 /48M = 0.895us

BUT, I found it will go into PDB1 sequence error interrupt handler. Then until I reduce the PWM frequence to 2KHz,  it will never go into the sequence error INT handler. I think it means the FTM0-TRGMUX-PDB1-ADC1  will cost at lease 500us. I want to know WHY.

0 Kudos
Reply
3 Replies

1,009 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

The calculation of a single ADC conversion time is correct.

But I would recommend routing the FTM trigger to a TRGMUX_OUTn pin as well and measuring the period of the trigger so that you can be sure this is correct.

Also, some ADC COCO triggers can be routed to TRGMUX_OUTn pins.

danielmartynek_0-1604068471516.png

Can you attach the whole project or a test code that would replicate the issue?

 

Regards,

Daniel

0 Kudos
Reply

1,002 Views
jxl
Contributor I

Dear Daniel,

         Thanks for your reply. My project is attached.

I toggle PD7 as test pin when ADC1 Interrupt and toggle again after read ADC1 data. Channel 0,1,2,3 are combine PWM, channel 4 is PD7.

jxl_0-1604133493388.png

If I change PWM frequency up to 100KHz, there will be a sequence error.

Look forward to your reply!Thanks very much!

 

0 Kudos
Reply

991 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Thank you for the project, but for some reason, I'm not able to run it.

I guess you use an old version of the Design Studio.

Can you show PDB registers after configuration?

 

Thanks,

BR, Daniel

0 Kudos
Reply