Are S32K1xx MCUs delivered with UART-Bootloader?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are S32K1xx MCUs delivered with UART-Bootloader?

Jump to solution
2,209 Views
DenisT1980
Contributor III

Or the first programming must be done via SWD-Interface?

0 Kudos
Reply
1 Solution
2,198 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
3 Replies
2,199 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there's no in-built bootloader, first programming must be done via SWD interface.

We provide these application notes about bootloaders:

https://www.nxp.com/docs/en/application-note/AN12218.pdf

https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip

 

https://www.nxp.com/docs/en/application-note/AN12323.pdf

https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip

Regards,

Lukas

 

0 Kudos
Reply
2,188 Views
DenisT1980
Contributor III

Thank you very much for your quick reply!

One more question:

is it possible to use the S32K146 Evaluation Board as SWD-Programmer for external modules based on S32K144 or S32K146 MCU's?

0 Kudos
Reply
2,177 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

That’s not expected usage. Theoretically it is possible, you could use connector for external debugger for wiring. The only problem I can see is that TDO signal is connected also to MCU on the EVB board, so there will be conflict between two output signals. It would be necessary to cut the TDO trace. I’m not really sure if the trace is easily accessible for such modification.

So, my statement is: no, it’s not recommended and it’s without our guarantees, of course.

Better option is:

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools/universal-mul...

and

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/universal-multilink-f...

(or see directly www.pemicro.com )

Both interfaces are compatible with S32DS

Regards,

Lukas

 

0 Kudos
Reply