Application run failure when launching debug or flash failure with J-flash V7.86e tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application run failure when launching debug or flash failure with J-flash V7.86e tool

1,375 Views
qinxk
Contributor I

ERROR: Timeout while preparing target, RAMCode did not respond in time (PC = 0x1FFF8002, XPSR = 0x01000000, SP = 0x1FFF8680)!
Failed to prepare RAMCode using RAM

0 Kudos
Reply
1 Reply

1,302 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @qinxk ,

   Thanks for your interest in the NXP S32K product, I would like to provide service for you.

    Sorry for the later reply, just get your question information.

    Please tell us, which S32K chip you are using? Tell us the detail chip partnumber, do you also test the NXP related chip RTD demo, whether that demo generate image use the JFLASH works or not?

   If you have the issues, you also can contact me through the email directly, I am kerry zhou, your valeo related China local auto MCU FAE, thanks.

Best Regards,

Kerry

0 Kudos
Reply