An error occurred during the installation of the tcpip package TCPIP_STACK _1_0_3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

An error occurred during the installation of the tcpip package TCPIP_STACK _1_0_3

ソリューションへジャンプ
450件の閲覧回数
suda1684
Contributor I

Dear Expert,

  My purpose is to obtain a demo with FreeRTOS + LwIP, so I go to install TCPIP_STACK.  

  When I installed Package TCPIP_STACK _1_0_3, the following error occurred.

suda1684_0-1702003157855.png

 Before that, I had already installed several software packages  on S32DS 3.5.

  •   SW32K3_S32DS_3.5.8_D2311
  •   SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite
  •   SW32K3_FreeRTOS_10_5_1_UOS_3_1_0_DS_updatesite_D2304

May I ask how to solve this problem?

Thanks.
suda

0 件の賞賛
返信
1 解決策
429件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

seems S32K396 development package is missing. Seems below thread is discussing this;
https://community.nxp.com/t5/S32K/tcpip-1-0-3-can-t-be-installed/m-p/1686564#M25052

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
430件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

seems S32K396 development package is missing. Seems below thread is discussing this;
https://community.nxp.com/t5/S32K/tcpip-1-0-3-can-t-be-installed/m-p/1686564#M25052

BR, Petr

0 件の賞賛
返信
401件の閲覧回数
suda1684
Contributor I

hi

  3q, this problem has been solved, I downloaded and installed the file SW32K39x_S32DS_3.5.6_D2309.zip.

0 件の賞賛
返信