AN5426: an external capacitor is added between the RESET pin to ground

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN5426: an external capacitor is added between the RESET pin to ground

523件の閲覧回数
jacky_Tan
NXP Employee
NXP Employee

Despite a capacitor in the reset line is not directly required for the MCU. In some cases, in order to add a further ESD protection,an external capacitor is added between the RESET pin to ground. The values of the pull up resistor and the capacitor must be selected according to the design requirements of the application. Refer to the device datasheet for the minimum RESET pulse value that can be detected for the MCU.

customer add 0.uf CAN in RESET pin to GND, it has download code issue.

customer need nxp to provide the CAP range? the  detail issue check attched file.

@Stephen Du <stephen.du@nxp.com>

 

 

0 件の賞賛
1 返信

516件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport
0 件の賞賛