AN5426: an external capacitor is added between the RESET pin to ground

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AN5426: an external capacitor is added between the RESET pin to ground

601 次查看
jacky_Tan
NXP Employee
NXP Employee

Despite a capacitor in the reset line is not directly required for the MCU. In some cases, in order to add a further ESD protection,an external capacitor is added between the RESET pin to ground. The values of the pull up resistor and the capacitor must be selected according to the design requirements of the application. Refer to the device datasheet for the minimum RESET pulse value that can be detected for the MCU.

customer add 0.uf CAN in RESET pin to GND, it has download code issue.

customer need nxp to provide the CAP range? the  detail issue check attched file.

@Stephen Du <stephen.du@nxp.com>

 

 

0 项奖励
1 回复

594 次查看
danielmartynek
NXP TechSupport
NXP TechSupport
0 项奖励