ADC with TRGMUX trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC with TRGMUX trigger

678 Views
1090097669
Contributor III

Hello everyone,

Based on the SDK, I want to use Trgmux-IN6 rising edge to trigger ADC sampling, but I can’t even get in the interrupt. The following are my configuration items:

1090097669_0-1611385059715.png

1090097669_1-1611385098576.png1090097669_2-1611385130241.png

 

1090097669_3-1611385405748.png

What's the problem?

Thanks

Tags (2)
0 Kudos
1 Reply

667 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

do you also select trgmux_in6 function at given pin? This is done in pin_mux component and TRGMUX tab. Then pin is configured after PINS_DRV_Init is called.

 

BR, Petr

0 Kudos