ADC value differences.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC value differences.

2,817 Views
daemangpark
Contributor I


Hi.
I use S32K144EVB. I think there are some differences between the input voltage and the value read by adc channel.
Test has been done under condition below.

SW : ADC_s32k144 (S32K example code)
HW : S32K144EVB

IDE : S32K design studio for ARM version 2018 R1.

1.Connect power from power supply to adc pin
2.Read caluated adc value.

results are as below.
(Input / caled value)
1.001V / 1018
1.101V /1125
1.201V /1224
1.5V /1531
2.001V /2047
2.501V /2561
3.001V /3075
3.501V /3594
4.001V /4103
4.500V /4626
4.800V /4925
5.000V /5000

The difference is growing when the input voltage goes to 5V.
I got 3 evb boards. and those gaps exist from All boards with the same SW (example codes).
Please check this out.#

0 Kudos
Reply
2 Replies

2,542 Views
daemangpark
Contributor I

Thanks Daniel. 

It much better doing after calibration. But the differences are still. ( 10~20 mA level).

Do you think it is working well?  Is it okay with these result? 10~20mA gap is acceptable? or any jobs are needed more?

Calibration has been done with API named ' void ADC_DRV_AutoCalibration(const uint32_t instance) '

The results are....

InputADC valueCalculatedDiff
10018179974
1501122614965
2001163519965
2501204124929
3001245129929
35012855348516
40013265398615
45003672448317
48003918478317
50004095498020

Please give your opinion.

BR.

Daemang Park.

0 Kudos
Reply

2,542 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Have you calibrated the ADC module?

Please refer to Section 42.5.6 Calibration function, S32K1xx_RM_rev7

Regards,

Daniel 

0 Kudos
Reply