ADC channel delay with SW trigger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC channel delay with SW trigger

ソリューションへジャンプ
1,621件の閲覧回数
ivaamonde
Contributor I

 

We are using Tresos 24.0.1 and MCAL 4.3 to configure the ADC with SW trigger. PDB is disabled.

documentation says that delay is related only to PDB trigger but it seems that the delay value affects conversion time.

Does channel delay apply when using SW trigger?

Which are the units of delay value? ADC clock ticks?

Thanks

0 件の賞賛
返信
1 解決策
1,606件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

There is a specific point in ADC SW Conversion in S32K MCAL: Even with SW trigger, the ADC still needs the PDB as a trigger (however PDB is triggered by SW). So you need to enable the PDB.

The channel delay is optional: You can setup a delay for PDB to trigger the ADC conversion, via "Adc Group Uses Channel Delays", or you can configure without delay, via "Adc Group In Back to Back Mode". The unit of delay value is ticks, based on one PDB tick. 

Best Regards,

Nam

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,607件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

There is a specific point in ADC SW Conversion in S32K MCAL: Even with SW trigger, the ADC still needs the PDB as a trigger (however PDB is triggered by SW). So you need to enable the PDB.

The channel delay is optional: You can setup a delay for PDB to trigger the ADC conversion, via "Adc Group Uses Channel Delays", or you can configure without delay, via "Adc Group In Back to Back Mode". The unit of delay value is ticks, based on one PDB tick. 

Best Regards,

Nam

0 件の賞賛
返信