ADC BCTU with PWM trigger using MCAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC BCTU with PWM trigger using MCAL

1,418 Views
Canberk
Contributor II

I wanna Start ADC conversion with PWM trigger and using BCTU. I use S32K344 board and I know there is a example named Adc_example_S32K344 for MCAL but it's complicated because it uses other configurations that I don't need like DMA. Is there any other example or documentation for this topic.

Thanks for help 

0 Kudos
Reply
1 Reply

1,406 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

There is also the Adc_Sar_Bctu_Ip_example_S32K344 example and in the AN13413 (4.2. Hardware triggers section) there is a brief description of ADC triggered from BCTU.

On the other hand, in MCSPTE1AK344 page there are app notes and sw for motor control that you can take as reference, where analogue data capturing is performed by ADC0, ADC1, BCTU and eMIOS peripherals.

Hope it helps you.

Have a nice day!

0 Kudos
Reply