ADC 2 instance for s32k344

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC 2 instance for s32k344

522 次查看
Ayaz
Contributor IV

Hi

I am triggering  the ADC at  each reload event of a pwm signal through the BCTU , the issue i am facing is that when i am triggering the ADC instance 2 at 40 kHz is working i can sample the data from the input , but when i am trying to sampling it at 2kHz there are no input , i do not have that issue at ADC 1 AND 2 instance, what do i miss here ?

i am using S32k344 .RTD 3.00

0 项奖励
回复
1 回复

498 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Ayaz

I can't give you a suitable solution from your description.

You need to provide a demo that can reproduce the problem so that we can help you

troubleshoot the cause of the problem.

0 项奖励
回复