Dear,all
when I USE 64 pins' S32K144 ,after change SDK & Package followed HOWTO: Change the CPU Derivative in an SDK-Based Application Project & How to change package on S32DS Processor Expert two documents.We enter default when the program runs to PINS_DRV_Init() , I hope somebody helps me.
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
Hi, I have met the same problem, how to solve it?
Hi, Bao!
Have u solved this problem? I'v encountered the same problem, if u have solved this problem, can u kindly share the solution? Thanks a lot!
Hi,
Can you give more details on which pins are configured and what clock sources are enabled?
Thank you,
Rares
Hi,Rares
PINs & clock source are the default configuration.
Executing the red marked program,program jump to b DefaultISR
Hi Tingkai,
Have you resolved this problem? Thanks!
Hi,
I was not able to reproduce the issue. Can you send me a simple project which I can use to reproduce it?
Also, what SDK version are you using?
Thank you,
Rares