关于K344 FlexIO模拟6路SENT接口参考例程

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于K344 FlexIO模拟6路SENT接口参考例程

1,108 Views
zhijian
Contributor I

hi,

       NXP是否有针对FlexIO模拟多通道SENT接口参考方案及配置参考例程(DMA方式),我们用到一个4+2的角度传感器(SENT接口),目前使用DMA配置一路SENT ,SNET信号能正确捕捉; 配置2路SNET后,2路SNET数据都为异常,1,2两路数据有会有交叉更新。针对FlexIO模拟多通道SENT(DMA方式)需要怎么配置?谢谢!

0 Kudos
Reply
4 Replies

1,079 Views
JoaquinL
NXP Employee
NXP Employee

Hi,

The sample project has been sent to the customer through FAE, and this post can be closed.

BR, Joaquin

0 Kudos
Reply

997 Views
abc1258
Contributor I
Hello,@ JoaquinL
I also need this routine, could you share a copy with me? Thank you
0 Kudos
Reply

986 Views
JoaquinL
NXP Employee
NXP Employee

Hi,

The K3 RTD 3.0.0 was released recently. You can try the example project of SENT driver in RTD.

This post was only for old version RTD and it may not work now.

Thank you!

BR, Joaquin

0 Kudos
Reply

968 Views
abc1258
Contributor I
ok ,thanks
0 Kudos
Reply