S32K知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K Knowledge Base

标签

讨论

排序依据:
******************************************************************************* The purpose of this demo application is to present a usage of the Hardfault handling for the S32K3xx MCU. ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** An example on S32K312: Read an unimplemented memory (0x80000):   volatile uint32_t read = *((uint32_t*)0x00080000); Hardfault will occur :--     Read Stack pointer when the HARDFAULT occur :-- SP = 0x2000ffd0 Go to this memory location , 0x2000ffd0 :--     When the program enters an exception handler, the stack frame is pushed onto the stack including the program counter value of the fault instruction.  At exception entry, the processor saves R0 R3, R12, LR, PC and PSR on the stack. hardfault occurred at, 0x00400e48, this is how to decode the address :--   Now How to reach this address 0x00400e48, using disassembly window :-- This is same place in main() function :-- volatile uint32_t read = *((uint32_t*)0x00080000);  
查看全文
S32K344 - Six-step commutation control These examples demonstrate a a 3-phase Brushless DC (BLDC) motor control drive using a Six-step commutation control with Hall position sensor and without any position sensor (sensorless). This design serves as an example of motor control design using NXP S32K3 automotive family. Examples were designed on S32K344 Brushless Direct Current and Permanent Magnet Synchronous Motor Control Development Kit.  C-project based examples are part of MCSPTE1AK344 Development Kit Application Software. An innovative drivers set, Real-Time Drivers (RTD),are used to configure and control the MCU. It complies with Automotive-SPICE, ISO 26262, ISO 9001 and IATF 16949. Production-ready Automotive Math and Motor Control Library set provides essential building blocks for algorithm. FreeMASTER is used as useful run-time debugging tool. Application software contains:  MCSPTE1AK344_BLDC_6Step_hall_ll-. Hall sensor-based example. Detailed description of the example can be found in attachment to this article MCSPTE1AK344 - 6-step hall.pdf. MCSPTE1AK344_BLDC_6Step_sensorless_ll – Sensorless based example. Detailed description of the example can be found in attachment to this article MCSPTE1AK344_- 6-step sensorless.pdf.   MATLAB Simulink based project (Motor Control BLDC Example - s32k344_mc_bldc_ebt) is build using Model-Based Design Toolbox (MBDT) and can be downloaded from NXP Model-Based Design Toolbox for S32K3xx - version 1.4.0 or newer releases.
查看全文
S32K344 - FOC integrated with FreeRTOS This example demonstrates a 3-phase Permanent Magnet Synchronous Motor (PMSM) vector control (Field Oriented Control - FOC) drive with 2- shunt current sensing with and without position sensor integrated in FreeRTOS environment. This design serves as an example of motor control design using NXP S32K3 automotive family. Example was designed on S32K344 Brushless Direct Current and Permanent Magnet Synchronous Motor Control Development Kit.  C-project based examples are part of MCSPTE1AK344 Development Kit Application Software. An innovative drivers set, Real-Time Drivers (RTD),are used to configure and control the MCU. It complies with Automotive-SPICE, ISO 26262, ISO 9001 and IATF 16949. Production-ready Automotive Math and Motor Control Library set provides essential building blocks for algorithm. FreeMASTER is used as useful run-time debugging tool. Application software contains:  MCSPTE1AK344_PMSM_FOC_2Sh_ll_FreeRTOS - Low-level drivers of RTD and S32 Design Studio Configuration Tools (S32CT) are used to demonstrate non-AUTOSAR approach. Since the motor control structure of the example is similar to dual shunt example, detailed description of the example can be found in application note AN13767 and FreeRTOS related part in AN12881 .
查看全文
S32K344 - FOC with dual single current measurement These examples demonstrate a 3-phase Permanent Magnet Synchronous Motor (PMSM) vector control (Field Oriented Control - FOC) drive with 1- shunt current sensing with and without position sensor. This design serves as an example of motor control design using NXP S32K3 automotive family.   Examples were designed on S32K344 Brushless Direct Current and Permanent Magnet Synchronous Motor Control Development Kit.  C-project based examples are part of MCSPTE1AK344 Development Kit Application Software. An innovative drivers set, Real-Time Drivers (RTD),are used to configure and control the MCU. It complies with Automotive-SPICE, ISO 26262, ISO 9001 and IATF 16949. Production-ready Automotive Math and Motor Control Library set provides essential building blocks for algorithm. FreeMASTER is used as useful run-time debugging tool. Application software contains:  MCSPTE1AK344_PMSM_FOC_1Sh_ll - Low-level drivers of RTD and S32 Design Studio Configuration Tools (S32CT) are used to demonstrate non-AUTOSAR approach. Since the structure of the example is similar to dual shunt example, detailed description of the example can be found in application note AN13767 and MCSPTE1AK344 - single shunt addendum.pdf (which highlights changes for single shunt)  attached to this article . MCSPTE1AK344_PMSM_FOC_1Sh_as_tr - RTD, EB (Elektrobit) tresos Studio and S32 Design Studio are used to demonstrate AUTOSAR (AUTomotive Open System ARchitecture) approach. Since the structure of the example is similar to dual shunt example, detailed description of the example can be found in application note AN13884 and MCSPTE1AK344 - single shunt addendum.pdf (which highlights changes for single shunt)  attached to this article .   MATLAB Simulink based project (Motor Control PMSM Single Shunt Example - s32k344_mc_pmsm_1sh_ebt) is build using Model-Based Design Toolbox (MBDT) and can be downloaded from NXP Model-Based Design Toolbox for S32K3xx - version 1.4.0 or newer releases.
查看全文
S32K344 - FOC with dual shunt current measurement These examples demonstrate a 3-phase Permanent Magnet Synchronous Motor (PMSM) vector control (Field Oriented Control - FOC) drive with 2- shunt current sensing with and without position sensor. This design serves as an example of motor control design using NXP S32K3 automotive family.   Examples were designed on S32K344 Brushless Direct Current and Permanent Magnet Synchronous Motor Control Development Kit.  C-project based examples are part of MCSPTE1AK344 Development Kit Application Software. An innovative drivers set, Real-Time Drivers (RTD),are used to configure and control the MCU. It complies with Automotive-SPICE, ISO 26262, ISO 9001 and IATF 16949. Production-ready Automotive Math and Motor Control Library set provides essential building blocks for algorithm. FreeMASTER is used as useful run-time debugging tool. Application software contains:  MCSPTE1AK344_PMSM_FOC_2Sh_ll - Low-level drivers of RTD and S32 Design Studio Configuration Tools (S32CT) are used to demonstrate non-AUTOSAR approach. Detailed description of the example can be found in application note AN13767. MCSPTE1AK344_PMSM_FOC_2Sh_as_tr - RTD, EB (Elektrobit) tresos Studio and S32 Design Studio are used to demonstrate AUTOSAR (AUTomotive Open System ARchitecture) approach. Detailed description of the example can be found in application note AN13884.   MATLAB Simulink based project (Motor Control PMSM Example - s32k344_mc_pmsm_ebt) is build using Model-Based Design Toolbox (MBDT) and can be downloaded from NXP Model-Based Design Toolbox for S32K3xx - version 1.4.0 or newer releases. Example is described in article  3-Phase Sensorless PMSM Motor Control Kit with S32K344 using MBDT blocks. 
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the LPI2C-0 as MASTER and LPI2C-1 SLave, using DMA for TX & RX for the S32K3xx MCU.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the Printf Semihosting for the S32K3xx MCU.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Create New project :-- Select Semi hosting library in project Properties :-- In Debugger setting :--- Include file :-- #include <stdio.h> Output :--    
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  SWT IP Driver for the S32K3xx MCU.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** With S32K312 device take care, HSE clock AIPS_SLOW_CLOCK ratio,  kept 1:2 :--   The example we use to trigger the SWT once & go to while(1) loop. This will trigger the watchdog RESET. Then After RESET from SWT we will check at starting of main function, if RESET reason is SWT, then glow LED and wait in while(1) loop  :--  
查看全文
******************************************************************************* The purpose of this demo application is to use pad keeping for  PINS and enter the standby mode & before entering the standby mode update variables in Standby RAM memory with pin state. Once wake up from the standby mode update the pins values from the STANDBY RAM variables.  S32K3xx MCU.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** =============== How this DEMO works ========== Before entring standby :-- Before entering standby mode, i make BLUE LED high SW6 on board pressed to enter the standby mode. Wakeup from Standby :-- SW5 on board pressed to wakeup from standby After wakeup from Stand by:-- I glow Green LED Unglow the BLUE LED Wait for SW6 on board to be pressed to enter the standby mode. ===============  Stand by RAM location =============== As noted, the Standby SRAM is allocated at the first 32 KB of the SRAM Memory. https://www.mouser.com/pdfDocs/S32K3MemoriesGuide.pdf =============== Pins used for PAD keeping =============== PTA30, PTA31, PTD14     =============== Switches used ===============   Enter Standby mode, by pressing SW6 on Board EXIT Standby mode, by pressing SW5 on Board =============== Wakeup source, SW5 PTB26 =============== =============== WKPU[41]  ---> WKPU_CH_45=============== Because First 4 WKPU are timers, so 41 + 4 = 45   =============== Linker file changed =============== Added Standby RAM memory & sections for standby RAM memory. Changes can be seen by comparing the original linker file      =============== Startup file changed , startup_cm7.s =============== Added call to Initialise the Standby RAM Changes can be seen by comparing the original startup_cm7.s file     ======================= How to verify if Standby RAM is working =============== 1> Declare two variables in file Wkup.c :-- __attribute__ ((section (".standby_ram_data"))) volatile int test_0_value ; __attribute__ ((section (".standby_ram_data"))) volatile int test_1_value ;   2> function set_pin_value() will be called before entering the standby mode. Initialise the values to these two variables inside function set_pin_value() in file Wkup.c.   3> Now burn the code inside the MCU using the PE micro debugger.     Once code is burned do not run the code & disconnect the debugger. 4> Power OFF and power ON the S32K312 board. Now code is waiting to enter standby mode. Press switch SW6 MCU will enter standby mode & Blue LED glowing. Press switch SW5 MCU will wakeup from the standby mode. Code will Now code is waiting to enter standby mode 5> Now open your debugger configuration, and attach to running target.   6> Once connected click on the ELF file & press pause button.   7> In Debug window you can see the value of variables test_0_value & test_1_value same as initialised before entering the standby mode.      
查看全文
This example for S32K312 is based on this, example on S32K344 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1732444 *******************************************************************************  The purpose of this demo application is to present a usage of the  ADC_SAR and BCTU IP Driver for the S32K3xx MCU.  The example uses the PIT0 trigger to trigger BCTU conversion list to  perform parallel conversions on ADC0/ADC1. Three ADC channels  are selected to be converted on each ADC:  ADC0: S8 , P0, S8  ADC1: S10, S13, S17  Converted results from BCTU FIFO are moved by DMA into result array.  ADC channel S10 is connected to board's potentiometer.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Set PIT Freeze Enable :--- BCTU will be do the parallel conversion for channel mentioned in BCTU list :--       "NEW DATA DMA enable mask" :-- controls These bit field in MCR register     "ADC target mask" :-- It controls "ADC_SEL " bit field in "Trigger Configuration (TRGCFG_0 - TRGCFG_71)" for single conversions you can enable only one instance so the possible values for target mask: 1 (0b001) ADC0 2 (0b010) ADC1 3 (0b100) ADC2| for list of conversions we can enable also parallel con version for example 3 (0b011) parallel conversion of ADC0 and ADC1 The trigger is configured as a list of parallel conversions ADC0, ADC1 in “Adc Target Mask”. List of ADC channels is defined in “BCTU List Items” while order is given by the “Adc Target Mask”: BctuListItems_0 is ADC0, BctuListItems_1 is ADC1 etc.     Result :-- I connected VDD from board on adc_0_p0 (PTD1 : J412-1)  and adc_1_p2 (PTE0 J412-13). Also POT value on S10 of ADC-1 & ADC-0-VREFH value coming correct & STABLE.     =========================Using  FIFO-2 ================= FIFO-2 Trigger & LIST Index :-- ADC channel conversion :--
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART6 for Freemaster uart Port. Freemaster project :-- S32K312_Freemaster_UART6\GUI_new\Project.pmpx  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************        
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the PORT & SIUL IP Driver for the S32K3xx MCU.  The example uses SW5 for switch debouncing.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  ADC_SAR IP Driver for the S32K3xx MCU.  The example uses the PIT0 trigger to trigger  conversions on ADC1.  ADC channels  are selected to be converted on  ADC-1:  ADC channel S10 is connected to board's potentiometer. #define ADC_SAR_USED_CH_BANDGAP 48U /* Internal Bandgap Channel */ #define ADC_SAR_USED_CH_POT_0 34U  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************      
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  FlexCAN IP Driver for the S32K3xx MCU.  The example uses FLEXCAN-0 for transmit & receive Tusing following Message buffer :-- #define RX_MB_IDX_0 10U #define RX_MB_IDX 11U #define TX_MB_IDX 12U FIFO Receive Message from range :-- 0x01 to 0x16 BAUDRATE : 500 KBPS  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the Siul2_Icu IP Driver for the S32K3xx MCU.  The example uses EIRQ-13 on PTB23 for interrupt..  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************        
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the DMA. MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART6 for transmit & receive five bytes using the DMA.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of   configure TRGMUX to select triggers for staring Normal/Injected chain conversion. Select PIT0_Ch0 as the hardware trigger source of ADC1_Ch34 & Ch48 via TRGMUX and two LEDs to show the trigger Sequence. ADC1_Ch34 is connected to board's potentiometer,Ch38 is bandgap channel.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q257 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: OpenSDA * Target: internal_FLASH ********************************************************************************
查看全文
*************************************************************************************************************** Detailed Description: Example shows implementation of Analog Comparator ‘45.7.5 Windowed mode (#s 5A & 5B)’ of S32K1XXRM using S32 SDK API. The Comparator is configured to compare analog input 0(AIN0) with half the reference voltage generated with the internal DAC. PDB is used to generate pulse output which is used as sampling windows of CMP block via TRGMUX. PDB period is 5ms, the first 2.5ms WINDOW=1 and the next 2.5ms WINDOW=0. Pdb0PulseOut not only be TRGMUX to Cmp0Sample but also to TrgmuxOut0, so that we are able to observe WINDOW at TRGMUX_OUT0(PTA1) pin. Based on the input from CMP0_IN0 (1kHz external triangle wave) the LEDs light by the following rules: 1) Vin < DAC voltage : RED on, GREEN off 2) Vin > DAC voltage : RED off, GREEN on 3) Unknown state : RED on, GREEN on EVB connection: Signal Function pin S32K144EVB-Q100 WINDOW TRGMUX_OUT0 PTA1 J5.5 2.5ms WINDOW=1 and 2.5ms WINDOW=0 Plus input CMP0_IN0 PTA0 J5.7 Need to connect external 1khz triangle wave COUTA CMP0_OUT PTE3 J1.16 square wave PTC1 PTC1 J5.13 If there is no external triangle wave, a square wave(PTC1) is generated and output to CMP0 (PTA1) * * ------------------------------------------------------------------------------------------------------------------------ * Test HW: S32K144EVB-Q100 * MCU: S32K144UAVLL 0N47T * Target: Debug_FLASH * Compiler: S32DS3.4 * SDK release: S32SDK_S32K1XX_RTM_4.0.3 * Debugger: PEMicro OpenSDA * ------------------------------------------------------------------------------------------------------------------------ Revision History: Ver   Date              Author            Description of Changes 1.0   Nov-9-2023   Robin Shen    Initial version, based on cmp_dac_s32k144 and pdb_periodic_interrupt_s32k144 ***************************************************************************************************************
查看全文
******************************************************************************** * Detailed Description: * The purpose of this example is show how to keep data in SRAM memory over SW * reset. SW reset is triggered by pressing the SW3 button on the S32K118EVB. * Reset is delayed for 514 LPO cycles. In the RCM interrupt, SRAMU_RETEN is * cleared allowing to retain SRAM data during the reset. After SW reset, * SRAMU_RETEN is set to allow accesses to SRAM. * File startup_S32K116.S in modified to skip ECC RAM initialization for SW reset * source. To check whether stored data stayed unmodified in the SRAM, specified * address is read and the LED lights up. * ------------------------------------------------------------------------------ * Test HW: S32K118EVB-Q064 * MCU: S32K118 LAMLH 0N97V QTZE1802B * Fsys: fsys = 48MHz * Debugger: Lauterbach Trace32 * Target: Debug * Terminal: 19200-8-no parity-1 stop bit-no flow control * EVB connection: default ******************************************************************************** Revision History: Ver Date Author Description of Changes 0.0 May-17-2023 David Tosenovjan Initial version *******************************************************************************/
查看全文