S32K知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K Knowledge Base

标签

讨论

排序依据:
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3x1 MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x47_A000   starting of FLS_CODE_ARRAY_0_BLOCK_0_S61.  ------------------------------------------------------------------------------ * MCU: S32K310 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Flash end address = 0x480000 Size of each block = 8192 = 0x2000 Start Address of 63 block = 0x480000 - 0x2000 = 0x47E000 = 4710400 Start Address of 62 block = 0x480000 - 0x4000 = 0x47C000 = 4702208 Start Address of 61 block = 0x480000 - 0x6000 = 0x47A000 = 4694016   Ram location where FLASH writing erase code is placed :-- I placed the code at 0x256 byte below the MAX address of the RAM size 16*1024 = 16384 = 0x4000 End of RAM = 0x20400000 + 0x4000 = 0x20404000  0x20404000 - 0x256 = 0x20403DAA 0x20403DAA = 541081002   Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00407b80 - 0x00407b54 = 0x2C = 44 byte  S32K3 FLASH Memory Terminology :--        
查看全文
 ------------------------------------------------------------------------------ * MCU: S32K310 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Example MCAL S32K310 MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K310 MEM_InFls DS3.5 RTD300 - NXP Community
查看全文
------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** S32K31XEVB-Q100 :-- S32K31XEVB-Q100 Evaluation Board for Automotive General Purpose | NXP Semiconductors Example MCAL S32K311 MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K311 MEM_InFls DS3.5 RTD300 - NXP Community
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3x1 MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x48_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************     Results :--     Ram location where FLASH writing erase code is placed :-- I placed the code at 256 byte below the MAX address of the RAM size 0x20407DAA = 541097386             Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00406ff0 - 0x00406f78 = 120 bytes                S32K3 FLASH Memory Terminology :--        
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3xx MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x50_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Results :-- Ram location where FLASH writing erase code is placed :-- I placed the code at 256 byte below the MAX address of the RAM size 0x20417DAA = 541162922     Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00407e64 - 0x00407e38 = 44 bytes      S32K3 FLASH Memory Terminology :--    
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the FEE MCAL Driver for the S32K3xx MCU. This example read & write 4 byte FEE BLock. I have renamed the FEE block using a MACRO as FOUR_BYTE_EEPROM_FEE_VARIABLE. The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x52_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
查看全文
------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300 :-- Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300 - NXP Community Example S32K344 UART Transmit & Receive Using Interrupt DS3.5 RTD300 :-- Example S32K344 UART Transmit & Receive Using Interrupt DS3.5 RTD300 - NXP Community
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART6 for transmit & receive five bytes using the Interrupt.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************         Putty output :--  
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART6 for transmit & receive five bytes using the DMA.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************     Putty output :--  
查看全文
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Example MCAL S32K312 MEM_InFls  DS3.5 RTD300 :-- Example MCAL S32K312 MEM_InFls DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE DS3.5 RTD300 :-- Example MCAL S32K312 FEE DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 - NXP Community    
查看全文
S32K344 - Six-step commutation control These examples demonstrate a a 3-phase Brushless DC (BLDC) motor control drive using a Six-step commutation control with Hall position sensor and without any position sensor (sensorless). This design serves as an example of motor control design using NXP S32K3 automotive family. Examples were designed on S32K344 Brushless Direct Current and Permanent Magnet Synchronous Motor Control Development Kit.  C-project based examples are part of MCSPTE1AK344 Development Kit Application Software. An innovative drivers set, Real-Time Drivers (RTD),are used to configure and control the MCU. It complies with Automotive-SPICE, ISO 26262, ISO 9001 and IATF 16949. Production-ready Automotive Math and Motor Control Library set provides essential building blocks for algorithm. FreeMASTER is used as useful run-time debugging tool. Application software contains:  MCSPTE1AK344_BLDC_6Step_hall_ll-. Hall sensor-based example. Detailed description of the example can be found in attachment to this article MCSPTE1AK344 - 6-step hall.pdf. MCSPTE1AK344_BLDC_6Step_sensorless_ll – Sensorless based example. Detailed description of the example can be found in attachment to this article MCSPTE1AK344_- 6-step sensorless.pdf.   MATLAB Simulink based project (Motor Control BLDC Example - s32k344_mc_bldc_ebt) is build using Model-Based Design Toolbox (MBDT) and can be downloaded from NXP Model-Based Design Toolbox for S32K3xx - version 1.4.0 or newer releases.
查看全文
S32K344 - FOC with dual single current measurement These examples demonstrate a 3-phase Permanent Magnet Synchronous Motor (PMSM) vector control (Field Oriented Control - FOC) drive with 1- shunt current sensing with and without position sensor. This design serves as an example of motor control design using NXP S32K3 automotive family.   Examples were designed on S32K344 Brushless Direct Current and Permanent Magnet Synchronous Motor Control Development Kit.  C-project based examples are part of MCSPTE1AK344 Development Kit Application Software. An innovative drivers set, Real-Time Drivers (RTD),are used to configure and control the MCU. It complies with Automotive-SPICE, ISO 26262, ISO 9001 and IATF 16949. Production-ready Automotive Math and Motor Control Library set provides essential building blocks for algorithm. FreeMASTER is used as useful run-time debugging tool. Application software contains:  MCSPTE1AK344_PMSM_FOC_1Sh_ll - Low-level drivers of RTD and S32 Design Studio Configuration Tools (S32CT) are used to demonstrate non-AUTOSAR approach. Since the structure of the example is similar to dual shunt example, detailed description of the example can be found in application note AN13767 and MCSPTE1AK344 - single shunt addendum.pdf (which highlights changes for single shunt)  attached to this article . MCSPTE1AK344_PMSM_FOC_1Sh_as_tr - RTD, EB (Elektrobit) tresos Studio and S32 Design Studio are used to demonstrate AUTOSAR (AUTomotive Open System ARchitecture) approach. Since the structure of the example is similar to dual shunt example, detailed description of the example can be found in application note AN13884 and MCSPTE1AK344 - single shunt addendum.pdf (which highlights changes for single shunt)  attached to this article .   MATLAB Simulink based project (Motor Control PMSM Single Shunt Example - s32k344_mc_pmsm_1sh_ebt) is build using Model-Based Design Toolbox (MBDT) and can be downloaded from NXP Model-Based Design Toolbox for S32K3xx - version 1.4.0 or newer releases.
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the FEE MCAL Driver for the S32K3xx MCU. This example read & write 4 byte FEE BLock. I have renamed the FEE block using a MACRO as FOUR_BYTE_EEPROM_FEE_VARIABLE.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Three FEE blocks are created. Each FEE block can be considered as EEPROM variables    How customer can use FEE block as EEPROM variable. Max size of FEE block :--     You can declare a MACRO for the Variable of EEPROM :-- FOUR_BYTE_EEPROM_FEE_VARIABLE How to Read and write the FEE variables :--  
查看全文
******************************************************************************************************* * Detailed Description: * DCF Record decouples CM7_0 and CM_1 on S32K344 * Find first available location in UTEST. * By default, first available address is 0x1B000768U * * NOTE: There is a bug in the RTD version. * Change FLS_MAX_VIRTUAL_SECTOR to 528 in C40_Ip_Cfg.h * ------------------------------------------------------------------------------ * Test HW: : S32K344EVB-Q257 * MCU: : S32K344 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * Autosar Conf.Variant : * SW Version : 4.0.0 * Build Version : S32K3_RTD_4_0_0_P20_D2403_ASR_REL_4_7_REV_0000_20240315 *******************************************************************************************************
查看全文
------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** S32K31XEVB-Q100 :-- S32K31XEVB-Q100 Evaluation Board for Automotive General Purpose | NXP Semiconductors S32K312 UART Transmit & Receive Using DMA :-- S32K311 UART Transmit & Receive Using DMA - NXP Community S32K311 UART Idle state Interrupt :-- S32K311 UART Idle state Interrupt - NXP Community
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART0 for transmit 20 packets with each packet of 21 bytes using the Interrupt in cyclic order. Also when receiving UART packet generate Idle interrupt when variable length of data is received. I used coolterm tool to send the string of data. If Data send by cool term is less than 20 bytes which is set by API call Lpuart_Uart_Ip_AsyncReceive(), then Ideal interrupt is received RTD driver modified in RTD --> Lpuart_Uart_Ip.c. Baudrate : 921600  ------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Idle Interrupt received :--    
查看全文
************************************************************************************************* * Detailed Description: * DCF record disables or enables POR_WDG depending on the POR_WDG_EN macro in main.c. * Find first available location in UTEST, by default, first available address is 0x1B000780 * * NOTE: There is a bug in this RTD version. * Change FLS_MAX_VIRTUAL_SECTOR to 272 in C40_Ip_Cfg.h * ------------------------------------------------------------------------------ * Test HW: : S32K312EVB-Q172 * MCU: : S32K312 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * Autosar Conf.Variant : * SW Version : 3.0.0 * Build Version : S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331 *************************************************************************************************
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART0 for transmit & receive 20 packets with each packet of 21 bytes using the DMA in cyclic order. Baudrate : 921600  ------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the Bootloader Jump to Application.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Jump is decided based on the boot_header, size we use to jump to the RESET handler:--   Cortex M-7 Interrupt vector table, RESET handler is 4 byte offset from starting of vector table :--       How to burn elf file of both application & bootloader code :--   Bootloader Linker file used :--   Application Linker file used :-- This linker file has provision to distribute RAM to both the cores   Application & bootloader both commented this, as CORE-1 should be started in CORE-0 main() function if required  :--   System.c file this changed (as in RTD-3.0.0 bug in startup file because of which HARDfault occurs in startup process for S32K324) :--  
查看全文
The S32K3 family of 32-bit AEC-Q100 qualified MCUs combines a scalable family of Arm® Cortex-M7-based microcontrollers built on long-lasting features with a comprehensive suite of production-grade tools. S32K3 MCUs are included in NXP’s Product Longevity Program, guaranteeing a minimum of 15 years of assured supply. The S32K3 offers dedicated peripherals set for rapid motor control loop implementation: enhanced Modular IO Subsystem(eMIOS), Logic Control Unit (LCU), TRGMUX, BodyCross-triggering Unit (BCTU), Analog to Digital Converter(ADC), and Analog Comparator (CMP). The comprehensive motor control ecosystem based on Automotive Math and Motor Control Library(AMMCLib) set, FreeMASTER with Motor Control ApplicationTuning (MCAT) tool and Model-Based Design Toolbox (MBDT) helps to enable S32K3 MCU in wide range of motor control use cases. The table below points to the articles with more detailed description each of S32K3 motor control use cases, hardware description, links to appropriate application notes and their addendums, and software repositories.  Device HW Article S32K344       MCSPTE1AK344 12 V development kit engineered for 3-phase PMSM and BLDC motor control applications     FOC with dual shunt current measurement Article focuses on solution based Field Oriented Control (FOC) technique (typically used for 3-phase PMSM motors) with dual shunt current measurement and without any position sensor (sensorless). The Encoder sensor is supported by SW option, but missing on HW kit. The available example codes covers both ANSI-C and Matlab Simulink approaches and uses RTD drivers with high-level Autosar complient API or low-level non-Autosar API.    FOC with single shunt current measurement Article focuses on solution based Field Oriented Control (FOC) technique (typically used for 3-phase PMSM motors) with single shunt current measurement and without any position sensor (sensorless). The Encoder sensor is supported by SW option, but missing on HW kit. The single shunt current measurement is advanced technique that allows decrese the cost of Bill of Material (BOM). The available example codes covers both ANSI-C and Matlab Simulink approaches and uses RTD drivers with high-level Autosar complient API or low-level non-Autosar API.    FOC integrated with FreeRTOS Article focuses on integration of motor control software (based on FOC with dual shunt current measurement) and Real Time Operating System (FreeRTOS). The available example code is based ANSI-C  code and uses RTD drivers with low-level non-Autosar API.    Six-step commutation control. Article focuses on solution based Six-step commutation (6-step) technique (typically used for 3-phase BLDC motors) with Hall position sensor and without any position sensor (sensorless). The available example codes covers both ANSI-C and Matlab Simulink approaches and uses RTD drivers with low-level non-Autosar API.    Note: the list of use cases cannot cover all combinations of MCU, current measurement scenario, control technique and sensor inputs, but should work as a base reference for most common configurations. This list is not final, please follow this acticle to be notified about updates with new use cases.   
查看全文