S32K3xx How to optimization APP code for get more high performance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K3xx How to optimization APP code for get more high performance

S32K3xx How to optimization APP code for get more high performance

Customer may need more high performance via S32K3xx. How to optimization user's code? 

As following have some suggestions: 

1. Most of user code allocate to P-Flash and enable I-Cache

2. Allocate system stack to D-TCM and enable D-Cache

3. Execute code frequently allocate to I-TCM. E.g., ISRs etc.

4. OS' task stack allocate to D-TCM

5. vector table allocate to D-TCM

Please note:

1. Due to enable D-Cache, other masters(E.g., DMA, HSE, another APP cores) access theses area of cacheable will be impact. So, theses area need to allocate to non-cacheable area.

2. If another master(E.g., DMA, HSE and another APP cores) access the D-TCM need to over back door. E.g., core1/DMA/HSE access core0' DTCM needed to over backdoor. 

Information:

S32K3' Coremark in RM, theses Coremark' value are from ARM. If used IAR/GHS etc and set compiler flag, then the Coremark value is very closely with RM. If used GCC, then the Coremark value will less than RM.

BR

Tomlin

 

 

无评分
版本历史
最后更新:
‎11-23-2023 11:58 PM
更新人: