S32K311 UART Transmit & Receive Using DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K311 UART Transmit & Receive Using DMA

S32K311 UART Transmit & Receive Using DMA

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 UART IP Driver for the S32K3xx MCU.

 The example uses LPUART0 for transmit & receive 20 packets with each packet of 21 bytes using the DMA in cyclic order.

Baudrate : 921600
 ------------------------------------------------------------------------------
* Test HW: S32K31XEVB-Q100
* MCU: S32K311
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Dinesh_Guleria_0-1712316250700.png



附件
无评分
版本历史
最后更新:
‎04-05-2024 04:26 AM
更新人: