Measure the running time of one function on S32K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Measure the running time of one function on S32K

Measure the running time of one function on S32K

Hi, 

      ARM Cortex-M have a DWT (Data Watchpoint and Trace) unit implemented, and it has a nice feature in that unit which counts the execution cycles. The DWT is usually implemented on most Cortex-M3, M4 and M7 devices, including e.g. the NXP S32K14x. 

    Attachment is the sample project on S32K142 to measure the running time of a function.

    Password of extraction is nxp.

    Enjoy the measuring!

 

Cheers!

Oliver

BTW, Measure the running time of one function on PowerPC could also be gotten through the link.

添付
100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎05-17-2020 08:58 PM
更新者: