Example S32K312 CAN Transmit & Receive Using MB Interrupt DS3.5 RTD300

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example S32K312 CAN Transmit & Receive Using MB Interrupt DS3.5 RTD300

Example S32K312 CAN Transmit & Receive Using MB Interrupt DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 FlexCAN IP Driver for the S32K3xx MCU.

 The example uses FLEXCAN-0 for transmit & receive using following Message buffer :--
#define RX_MB_IDX_0 10U
#define RX_MB_IDX 11U
#define TX_MB_IDX 12U



BAUDRATE : 500 KBPS

 ------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

 

Dinesh_Guleria_0-1709212705051.png

 

Dinesh_Guleria_1-1709212743552.png

 

Dinesh_Guleria_2-1709212752282.png

 

添付
コメント

@Dinesh_Guleria ,

I'm unable to download this project due to permission issue.

Please share or upload the downloadable one.

Thank you,

評価なし
バージョン履歴
最終更新日:
‎02-29-2024 06:22 AM
更新者: