Example S32K144 DMA memory copy test S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example S32K144 DMA memory copy test S32DS

Example S32K144 DMA memory copy test S32DS

********************************************************************************
* Detailed Description:
*
* This example shows how to init DMA for simple memory to memory copy.
* Eight 16-bit values are copied upon SW start.
*
* ------------------------------------------------------------------------------
* Test HW:         FRDM-S32K144
* MCU:             PS32K144HFVLL 0N77P
* Fsys:            default
* Debugger:        S32DS
* Target:          internal_FLASH
*
********************************************************************************

Original Attachment has been moved to: Example-S32K144-DMA-RAM2RAM-test-v1_0-S32DS.zip

标签 (1)
评论

Could you send this example? The linkage is invalide. Thanks

CY9
 
Invalid Parameters Specified

 

An invalid set of parameters has been specified in the url.
 
50% 有帮助 (1/2)
版本历史
最后更新:
‎10-14-2016 01:22 AM
更新人: