*******************************************************************************************************
Detailed Description:
Configures the MCU to run system clock from XOSC.
LPUART1 is set to respond to LIN header sent from master.
Based on ID received the LPUART1 either receive frame's data and compare checksum
or publish requested data with calculated checksum. Enhanced checksum is used.
Interrupt is used for RX and TX operation and 2 versions of interrupt routine are available.
VER 1 ... during response transmission receiver disabled and transmit interrupt enabled
VER 2 ... during response transmission receiver is kept enabled
------------------------------------------------------------------------------
Test HW: S32K116 EVB-Q048
MCU: PS32K116LAM 0N96V
Fsys: 40MHz
Debugger: Lauterbach
Target: internal_FLASH
******************************************************************************************************
Hi Petr ,
You had used PTD5 as LIN sleep enable pin, but in schematic S32K116 EVB-Q048 LIN transrecevier sleep pin is pulled up to +ve .
Do we need to set PTD5 pin ?
Hi Petr ,
I am developing LIN Master using S32K116EVB-Q048 , is FlexIO configuration is mandatory in LIN Master ?
If yes, can you explain the how to configure FLEXIO->TIMCMP[0] register .Using SIRCDIV2 clock @8MHz for FlexIO module.
Regards ,
Yogish