Example S32K116 FlexCAN VLPR test S32DS.ARM.2.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example S32K116 FlexCAN VLPR test S32DS.ARM.2.2

Example S32K116 FlexCAN VLPR test S32DS.ARM.2.2

********************************************************************************
 Detailed Description:

 Example shows FlexCAN 0 usage in RUN/VLPR modes using SDK.
 CAN bitrate is set to 250bit/s.

 MCU enters VLPR mode by pressing SW3 button. CAN std message is sent with data VLPRmode"
 MCU exits VLPR to RUN mode when one of following happens:
 - CAN std message with RX_MSG_ID is received and MCU is in VLPR
 - SW2 button is pressed (PTC12 interrupt). CAN std message is sent with data "RUN mode"

 Blue LED is dimming and the rate is different for each power mode due to different
 system clock (48Mhz vs 4MHz)

 ------------------------------------------------------------------------------
 Test HW: S32K116EVB-Q48
 MCU: PS32K116LAM 0N96V
 Compiler: S32DS.ARM.2.2
 SDK release: S32SDK_S32K1xx_RTM_3.0.3
 Debugger: Lauterbach, OpenSDA
 Target: internal_FLASH

********************************************************************************

附件
无评分
版本历史
最后更新:
‎12-03-2020 01:46 AM
更新人: