using configtool on S32 Design studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

using configtool on S32 Design studio

1,492 次查看
sangrael
Contributor I

Hi NXP,

 

I am just trying to configure all comms and GPIOs on S32G274A chip using configtool on S32 Design studio.

 

It says MCU is not selected. 

 

Could you help me out?

 

Regards,

Sangrae

0 项奖励
回复
3 回复数

204 次查看
Petro
Contributor I

Same problem with S32K144. The project is created, compiled, and loaded, but ConfigTool it doesn't see the processor target.

0 项奖励
回复

1,482 次查看
asap
NXP Employee
NXP Employee

Hi Sangrae,

You could open S32DS (ver3.4 or later), create a S32DS application project->select the right core you are using -> add the SDK(RTD) for each of the core (if you are using M7). if RTD not yet installed, please install RTD to S32DS also. 

You could refer to the S32G training hub (S32G2 Technical overview) for more detail guide. 

Albert
0 项奖励
回复

174 次查看
Petro
Contributor I

Where can I get an RTD? It's not in the extension list.

0 项奖励
回复