unable to boot both A53 and M7 core in S32G2 by following "multicore enablement guide"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unable to boot both A53 and M7 core in S32G2 by following "multicore enablement guide"

705件の閲覧回数
Lee0202
Contributor III

i am working on " multicore enablement guide " where I am using same version packages and everything. i did from building U-boot to flashing images flashing images to NOR -flash. I didn't get any prompt terminal after flashing. Iam suspecting the following deviations may be reasons, if not please let me know.

1)while building ATF

my log file load address are these:

IVT Location: SD/eMMC
Load address: 0x342fc680
Entry point: 0x34302000

but in document values are:

IVT Location: SD/eMMC
Load address: 0x342fc580
Entry point: 0x34302000

load address got deviated

2)IPCF while building got some errors, but any way   . ko files generated and kept in FAT32 (boot_s32g27).

3)I got only IPCF examples for only M7_core_0 and M7_core_1 in DS studios but not for M7_core_2.

4)I didn't disable or removed both RM plugin and RM_init in EBtresos (because i got header file missing error while "Generating Project")

5)While making final IVT address configuration, after making "Generate S32G Boot Image Using S32DS IVT_TOOL". Initially it is deviated later I forcefully aligned as per the Document image.

 

Please find the Document attached below." Let me what is the problem why Iam not getting anything in terminal after following " multicore enablement guide" .

タグ(1)
0 件の賞賛
返信
1 返信

670件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Lee0202 

Seems this issue is similar to the other post from your side, which has been replied, may I know if we could discuss it at one side?

Thanks

Best Regards

Chenyin

0 件の賞賛
返信