source.codeaurora.org is unavailable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

source.codeaurora.org is unavailable

Jump to solution
1,763 Views
jiahaisheng
Contributor I

I am in the github codebase:

https://github.com/nxp-auto-linux/ipc-shm-us/tree/release/SW32R45_IPCF_4.4.0_D2303

To download the code for /ipc-shm-us/common/,

use the command: git submodule update --init --recursive

will indicate fatal: unable to access 'https://source.codeaurora.org/external/autobsps32/ipcf/ipc-shm/': Could not resolve host: source.codeaurora.org,

how do I get the code under ipc-shm-us/common/?

Thanks!

0 Kudos
Reply
1 Solution
1,672 Views
nxf92108
NXP Employee
NXP Employee

Hi,

Yes, ipc-shm-us/common is the code from ipc-shm/.

Please, let us know.

View solution in original post

2 Replies
1,756 Views
jiahaisheng
Contributor I

Or is the code under ipc-shm-us /common/ the code under ipc-shm/?

0 Kudos
Reply
1,673 Views
nxf92108
NXP Employee
NXP Employee

Hi,

Yes, ipc-shm-us/common is the code from ipc-shm/.

Please, let us know.