Hi,
In the current configurations, few FCCU faults are configured with R1 reaction in the eMcem module.
While configuring FCCU tests in sBoot, no R1 configuration is available. Only R1_R2 is available.
When configured for R1_R2, it's expecting that NMI shall be enabled, which will result in a reset for the current application.
How can I configure only R1 for the sBoot FCCU NCF test?
SAF version: SW32G_SAF_2.0.2_QLP01_D2410
Hello, @Irshad2225
Thanks for the post.
I just check the code of sBoot.
There is not R1 only reaction defined, so that it cannot be set to R1
I feel sorry for your inconvenience.
BR
Chenyin